:MHIStogram:ASCii:DATA?

Query Syntax

:MHIStogramN:ASCii:DATA?

Where N identifies one of four possible measurement histograms {1:4}. For example, :MHIStogram3.

Description

Returns the histogram database as ASCII data (comma-separated values).

Each value is the number of hits (measurement results) in the histogram bin.

To query the number of bins in the measurement histogram, use the :MHIStogram:POINts? query.

To return the data in binary, use the :MHIStogram:INTeger:DATA? query.