:WMEMory:EYE:CURSor
Command Syntax
:WMEMoryN:EYE:CURSor <symbol_0_position>
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
<symbol_0_position> is an integer from 0 to 15.
Query Syntax
:WMEMoryN:EYE:CURSor?
Description
When qualifying a real-time eye with symbols in a 16-character pattern (see :WMEMory:EYE:BITS), this command selects the position of symbol 0 in the pattern. Depending on which position you select for symbol 0, the pattern can include symbols before, after, or both before and after symbol 0. Position 0 means all symbols in the pattern are before symbol 0. Position 15 means all symbols in the pattern are after symbol 0.
To specify the pattern, see the :WMEMory:EYE:PATTern command.