:WMEMory:EYE:WINDow:METHod
Command Syntax
:WMEMoryN:EYE:WINDow:METHod {EOPening | CLOCk}
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:EYE:WINDow:METHod?
Description
This command specifies how the eye window used for measurements is determined:
-
EOPening— Measures within an eye window defined by left and right opening locations.Use the
:WMEMory:EYE:WINDow:LEFTand:WMEMory:EYE:WINDow:RIGHtcommands to specify the left and right opening location values. The default values are 40% (left) and 60% (right) which identifies the central 20% of symbol period. -
CLOCk— Measures within an eye window that is a width percentage at the location of the recovered clock edge.Use the
:WMEMory:EYE:WINDow:WIDThcommand to specify the width percentage value.
This command is equivalent to the settings in the Eye tab of the Configure Measurements dialog box.