:WMEMory:EYE:UIXPosition
Command Syntax
:WMEMoryN:EYE:UIXPosition <time_in_UI>
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
<time_in_UI> is a double in UI (unit interval) units.
Query Syntax
:WMEMoryN:EYE:UIXPosition?
Description
Sets the waveform memory N horizontal time position (center display location) of the real-time eye display in UI units.
This command directly affects the real-time eye's horizontal position setting in seconds (see the :WMEMory:EYE:XPOSition command).
To set the horizontal time range of the real-time eye display in UI units, use the :WMEMory:EYE:UIXRange command.