:WMEMory:EYE:UUNits
Command Syntax
:WMEMoryN:EYE:UUNits {UINTerval | SECond}
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:EYE:UUNits?
Query Response
{UINT | SEC}
Description
This command specifies the user interface's units option for the real-time eye horizontal Scale and Position controls. You can select either Unit Intervals (UIs) or time (in seconds).
To specify the real-time eye horizontal scale and position in terms of UI units, use the :WMEMory:EYE:UIXRange and :WMEMory:EYE:UIXPosition commands.
To specify the real-time eye horizontal scale and position in terms of time units, use the :WMEMory:EYE:XSCale and :WMEMory:EYE:XPOSition commands.