:WMEMory:EYE:XSCale
Command Syntax
:WMEMoryN:EYE:XSCale <seconds_per_div>
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
<seconds_per_div> is a double.
Query Syntax
:WMEMoryN:EYE:XSCale?
Description
Sets the waveform memory N horizontal time scale of the real-time eye display in seconds-per-division.
This command directly affects the real-time eye's horizontal range setting in UI (unit interval) units (see the :WMEMory:EYE:UIXRange command).
To set the horizontal position (center display location), use the :WMEMory:EYE:XPOSition command.
Only the center UI is valid for the recovered clock edge. You can display up to 10 UIs to show context before and after the center UI.