:WMEMory:EYE:DISPlay
Command Syntax
:WMEMoryN:EYE:DISPlay {ON | OFF | 1 | 0}
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:EYE:DISPlay?
Query Response
{1 | 0}
Description
Turns the display of the specified waveform memory's real-time eye on or off. Use the :WMEMory:STATus? command to determine if a channel is available for display.
Use an *OPC (Operation Complete) query to pause program execution while waiting for this command to complete.