:WMEMory:EYE:WINDow:WIDTh
Command Syntax
:WMEMoryN:EYE:WINDow:WIDTh<percent>
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
<percent> is a double.
Query Syntax
:WMEMoryN:EYE:WINDow:WIDTh?
Description
When the "At Clock Time" eye window determination method is selected (see :WMEMory:EYE:WINDow:METHod), this command specifies the UI percentage width about the recovered clock location to use as the eye window. A zero percent for this setting means only the recovered clock location is used.
This command is equivalent to the settings in the Eye tab of the Configure Measurements dialog box.