:WMEMory:EYE:XPOSition
Command Syntax
:WMEMoryN:EYE:XPOSition <time>
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
<time> is a double.
Query Syntax
:WMEMoryN:EYE:XPOSition?
Description
Sets the waveform memory N horizontal time position (center display location) of the real-time eye display.
This command directly affects the real-time eye's horizontal position setting in UI (unit interval) units (see the :WMEMory:EYE:UIXPosition command).
To set the horizontal time scale of the real-time eye display in seconds-per-division, use the :WMEMory:EYE:XSCale command.