Last updated: January 16, 2009
This section is only applicable to the lab application.
 Out-of-Synch Handling of Output Power 
measurement does not return any measurement results at this time. Initiating the measurement only causes the test set to change its DPCCH_Ec/Ior as specified by the 
Out-of-Synch Handling of Output Power Measurement Parameters
. You must use an external spectrum analyzer to measure the UE's resulting output power. When the
 Out-of-Synch Handling of Output Power 
measurement is initiated from the test set, the test set generates a trigger at point A that you can route to the test set's rear panel
 TRIG OUT 
connector using the 
Trigger Output Setup
 setting, to trigger the spectrum analyzer. See 
How Do I Make an Out-of-Synch Handling of Output Power Measurement?
.
 Measurement Generated
.
Connected DL Channel Levels 
as specified by 3GPP TS 34.121 Table E.3.3 and Table 5.4.4.3:
Cell 1 Connected CPICH Level 
=
 -10.00 dB
.
Cell 1 Connected P-CCPCH/SCH Level 
=
 -12.00 dB
.
Cell 1 Connected S-CCPCH Level 
=
 Off
.
Cell 1 Connected PICH Level 
=
 -15.00 dB
.
Cell 1 Connected DPCH Level 
=
 -16.60 dB
. (This sets DPCCH_Ec/Ior before point A to -16.6 dB, because PO1 = PO2 = PO3 = 0, which makes DPCH_Ec/Ior = DPCCH_Ec/Ior).See Downlink Channel Levels .
 All Up bits
.
 Call Parms 1 of 3 
menu) to
 -61 dBm
.
 Generator Info 
(
F3
 on the
 Call Control 2 of 5 
menu) and set 
AWGN Power
 (
F5
) to
 -60 
dBm.The out-of-synch handling of output power measurement can be performed while in FDD Test Operating Mode , however you must configure the UE such that its output power will respond appropriately to the changes in the test set's DPCCH_Ec/Ior.
 Cell 1 Connected DPCH Level 
is less than Qin.
 Measurement Timeout 
> 
Segment Ta-b Interval
 + 200 ms + 
Segment Tc-d Interval
 + 
Segment Td-e Interval
 + 200 ms.