:ACQuire:SPBit:MODe
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :ACQuire:SPUI:MODE command.
Command Syntax
:ACQuire:SPBit:MODe {AUTomatic | MANual}
Query Syntax
:ACQuire:SPBit:MODe?
Description
When the entire pattern is acquired (:ACQuire:EPATtern), use this command to select automatic or manual entry of samples-per-bit. Changing the samples-per-bit affects sweep time (display update rate), histograms, and measurements.
- AUTomatic
- FlexDCA sets the record length to optimize the single record length versus total database update rate. Automatic is the default setting. It is recommended to select automatic when in color grade or gray scale waveform persistence, or a histogram, or a mask test is enabled.
- MANual
- Allows you to set the actual sample number using the
ACQuire:SPBitcommand.
Requires FlexDCA revision A.01.80 and above.