:ACQuire:SPUI:MODE
Instrument:
N1010A
N1000A
DCA-M
UXR Scope
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:ACQuire:SPBit:MODe {AUTomatic | MANual}
Query Syntax
:ACQuire:SPBit:MODe?
Description
Select between AUTomatic or MANual entry of Samples / UI (record length). Changing the Samples / UI affects sweep time (display update rate), histograms, and measurements.
- AUTomatic
- FlexDCA sets the record length to optimize the single record length versus total database update rate. Automatic is the default setting. It is recommended to select automatic when in color grade or gray scale waveform persistence, or a histogram, or a mask test is enabled.
- MANual
- Allows you to set the actual sample number using the
ACQuire:SPUIcommand.
Requires FlexDCA revision A.05.60 and above.
This command replaces deprecated command :ACQuire:SPBit:MODe.