:CALibrate:FRAMe:PTIMebase:STATus:DTEMperature?
Instrument
N1000A-PTB
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:FRAMe:PTIMebase:STATus:DTEMperature?
Description
Returns a string from a DCA-X that provides the change in temperature (Celsius) of the DCA-X since the last internal precision timebase calibration. Use the :CALibrate:FRAME:PTIMebase:STATus? parent query to determine if a calibration is needed. Use the :CALibrate:FRAME:PTIMebase:STARt command to calibrate the internal precision timebase.
The following is an example of the returned string, which indicates that the temperature of the N1000A has risen 1.04°C:
"1.040000000E+00"
Requires FlexDCA revision A.03.00 and above and an N1000A-PTB instrument, which includes an internal precision timebase.