:CALibrate:FRAMe:PTIMebase:STATus:TIME?
Instrument
N1000A-PTB
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:FRAMe:PTIMebase:STATus:TIME?
Description
Returns a string from a DCA-X that provides the time that has elapsed since the last DCA-X internal precision timebase calibration. Use the :CALibrate:FRAME:PTIMebase:STATus? parent query to determine if a calibration is needed. Use the :CALibrate:FRAME:PTIMebase:STARt command to calibrate the internal precision timebase.
The following is an example of the returned string:
"01/09/2014 06:20:09"
Requires FlexDCA revision A.03.00 and above and an N1000A-PTB instrument, which includes an internal precision timebase.