:CALibrate:FRAMe:TIMebase:STATus:DETails?
Instrument
N1000A
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:FRAMe:TIMebase:STATus:DETails?
Query Response
"<details>"
Description
Returns a string that provides the date of the last Mainframe Factory Timebase calibration as well as the elapsed time and the temperature (Celsius) change. Use the :CALibrate:FRAME:TIMebase:STATus? parent query to determine if a calibration is needed. Use the :CALibrate:FRAME:TIMebase:STARt command to calibrate the timebase.
Examples of Returned Status String
"Time of last Calibration: 01/09/2014 06:20:09,Elapsed Calibration Time: 8 days,Temperature Change: 1.04 C"
Requires FlexDCA revision A.03.00 and above.