:CALibrate:FRAMe:TIMebase:STATus:TIME?
Instrument
N1000A
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:FRAMe:TIMebase:STATus:TIME?
Query Response
"<time>"
Description
Returns a string that provides the time that has elapsed since the last Mainframe Factory Timebase calibration. Use the :CALibrate:FRAME:TIMebase:STATus? parent query to determine if a calibration is needed. Use the :CALibrate:FRAME:TIMebase:STARt command to calibrate the timebase.
Example Returned Status String
10/08/2018 15:01:32"
Requires FlexDCA revision A.03.00 and above.