:CALibrate:FRAMe:TIMebase:STATus:DTEMperature?
Instrument
N1000A
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:FRAMe:TIMebase:STATus:DTEMperature?
Query Response
<delta temperature>
Description
Returns a number that provides the change in temperature (Celsius) of the mainframe since the last Mainframe Factory Timebase calibration. Use the :CALibrate:FRAME:TIMebase:STATus? parent query to determine if a calibration is needed. Use the :CALibrate:FRAME:TIMebase:STARt command to calibrate the timebase.
Example Returned Status String
3.24E+00
Requires FlexDCA revision A.03.00 and above.