:CALibrate:CONTinue

Flex Apps:
FlexDCA
FlexRT

Command Syntax

:CALibrate:CONTinue

Description

Continues all calibrations that are in process. As a calibration progresses, message or decision dialogs often appear. For example, the user might be instructed to disconnect any front-panel inputs to a module. This command is equivalent to clicking the dialog's Next or Done button. Use the CALibrate:CANCel command for an equivalent of the Cancel button. Use the :CALibrate:SDONe command to pause your application until the user clicks a button and to determine the which button was pressed.

Example Command Sequence

The following commands are used for a typical vertical calibration.

:CALibrate:SLOT3:STARt
:CALibrate:SDONe?
:CALibrate:CONTinue    //  Dismiss the begin notice calibration dialog
:CALibrate:SDONe?
:CALibrate:CONTinue    //  Dismiss the disconnect notice dialog
:CALibrate:SDONe?
:CALibrate:CONTinue    //  Dismiss calibration complete dialog
*OPC?