:CALibrate:SLOT:STATus:TIME?
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:SLOT{1:8}:STATus:TIME?
Where the required specifier {1:8} identifies a specific module by slot number. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1.
Description
For the indicated slot, determines the oldest date and time between the last vertical calibration, precision timebase, or clock recovery calibrations and returns the value. If a calibration has not yet been performed, an empty string is returned.
Example Returned Status String
"03/22/2012 14:52:00"
Example Command
:CALibrate:SLOT3:STATus:TIME?