:CHANnel:ATTenuator:RESet
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CHANnel{1:8}{A|B|C|D}:ATTenuator:RESet
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Resets the attenuation compensation factor to 0 (1:1). For more information on attenuation factors, refer to the :CHANnel:ATTenuator:STATe command.
Requires FlexDCA revision A.01.80 and above.
Example Command
:CHANnel2A:ATTenuator:RESet