:CHANnel:CONNector
Removed command. Starting with FlexDCA revision A.08.30 and above, the 86115D module was obsoleted.
Command Syntax
:CHANnel{1:8}{A|B|C|D}:CONNector {A | B | NAPPlicable}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:CONNector?
Description
For 86115D Option 004 modules, selects the optical input connector for the channel. The 86115D with option 004 has two connectors per channel. When a channel's alternate connector is selected, all the vertical settings of the current connector (for example scale, offset, wavelength, filter) will be applied to the newly selected connector. This command is not available for 86115D Option 002 modules, as these modules have only one connector available for each channel.
When queried, one of the following responses is returned:
- A
- Connector A is selected as the channel input.
- B
- Connector B is selected as the channel input.
- NAPPlicable
- An 86115D option 004 module is not installed in the N1000A.
Example Command
:CHANnel2A:CONNector:A