:CHANnel:PROBe:STATe

Command:
Deprecated
Flex Apps:
FlexDCA
FlexRT

Removed command. Starting with FlexDCA revision A.08.30 and above, the 86xxx-series, 83xxx-series, and 54xxx-series modules have been obsoleted.

Command Syntax

:CHANnel{1:8}{A|B|C|D}:PROBe:STATe {ON | OFF}

Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).

The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.

Query Syntax

:CHANnel{1:8}{A|B|C|D}:PROBe:STATe?

Description

Queries a response that indicates if a probe is connected to a channel input. To specify the model of a probe that is connected to a channel, use the :CHANnel:PROBe:ID command.

Requires FlexDCA revision A.02.00 and above.

Example Command

:CHANnel2A:PROBe:STATe ON