:CHANnel:YBOTtom?
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CHANnel{1:8}{A|B|C|D}:YBOTtom?
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Queries the amplitude value represented by the graticule's bottom edge. To query the amplitude value represented by the graticule's top edge, use :CHANnel:TOP?. Use the :CHANnel:YSCale command to set the amplitude scale value in volts or Watts. Use the :CHANnel:YOFFset command to set the amplitude offset.
Example
:CHANnel2A:YBOTtom?