:CHANnel:YUNits
Command Syntax
:CHANnel{1:8}{A|B|C|D}:YUNits {VOLT | WATT | AMPere | UNKNown}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:YUNits?
Description
Sets or queries the waveform's vertical units, which can be either volts, Watts, amperes, or unknown. Amperes can be selected when an external transducer is connected to an electrical the input channel. Use the :CHANnel:TRANsducer:STATe and :CHANnel:TRANsducer:UNITs commands for this task.
The command form was added to the query form starting with FlexDCA revision A.04.00 and above.
Example Command
:CHANnel2A:YUNits WATT