:DISK:IREPort:FNAMe:USTandard
Flex Apps:
FlexDCA
FlexPLL
Command Syntax
:DISK:IREPort:FNAMe:USTandard
Description
Resets the file name for the Instrument Report file from using a custom name to using the standard name in the following form:
InstrumentReport_<date><autonumber>.<extension>
For example, InstrumentReport_2022-10-23_1.xps. Refer to :DISK:IREPort:FNAMe to learn about standard and custom names.
Requires FlexDCA revision A.07.60 and above.