:EMODules:CRECovery:SADDress
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:EMODules:CRECoveryN:SADDress <SICL address>
Where N identifies slot number {1:8} which is associated with clock recovery module. On 86108A modules, specify slot 1.
<SICL address> is a string.
Query Syntax
:EMODules:CRECoveryN:SADDress?
Description
Specifies the SICL address of an extended module, such as an N4877A clock data recovery and demultiplexer. To specify a VISA address, use the :CRECovery:VADDress
command. Use the :SLOT:ADDRess
command to select the type of address. Use the :SLOT:CONNect command to actually establish the LAN connection.
Requires FlexDCA revision A.02.00 and above.