:EMODules:SLOT:ADDRess

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:EMODules:SLOT{1:8}:ADDRess {SICL | VISA | RS232}

Where the {1:8} specifier identifies a specific module by slot.

Query Syntax

:EMODules:SLOT{1:8}:ADDRess?

Description

Specifies the interface type to a supported extended module: LAN, RS-232, or none. The following table lists the interfacee selections for each type of extended module. Use the commands in the table to actually enter the address of the extended module. Do not use this command for simulated or the N1000A configured as an extended module. For the N1000A, use the commands in the :RDCA subsystem.

Commands for Entering LAN Addresses
Extended Module Supported Interface Commands
SICL Address VISA Address USB RS-232
N1000A Use the :RDCA subsystem commands
N109xA-series DCA-M — — automatically detected —
N107xA-series DCA-M — — automatically detected —
Optical Switch :EMODules:SWITch:SADDress :EMODules:SWITch:VADDress automatically detected :EMODules:SWITch:PORT
M8195/6A AWG :EMODules:AWGenerator:SADDress :EMODules:AWGenerator:VADDress automatically detected —
Simulated None

Requires FlexDCA revision A.06.00 for the M8195A and M8196A. For other extended modules, requires FlexDCA revision A.02.00 and above.

Example Command

:EMODules:SLOT4:ADDRess VISA