:JSAMemory:PLLoop:MODE?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Query Syntax
:JSAMemory:PLLoop:MODE?
Query Response
{JTF | OJTF}
Description
From the JSA memory database, returns the clock recovery emulation's type of first- or second-order PLL transfer function. The setting can be a Jitter Transfer Function (JTF) or Observed Jitter Transfer Function (OJTF).
JSA requires an 86108A/B module with Option JSA. To use JSA in Jitter Mode, L-RND package license (includes feature F-JIT Enhanced Jitter Analysis) is required.
Requires FlexDCA revision A.02.50 and above.