:JSAMemory Subsystem

Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT

Use the JSAMemory subsystem commands to view, use, or query the data within the JSA Memory database. These commands correspond to features that are shown on the JSA Memory dialog. To use Jitter memory (versus JSA memory), use the :JDMemory subsystem.

JSA requires an 86108A/B module with Option JSA. To use JSA in Jitter Mode, L-RND package license (includes feature F-JIT Enhanced Jitter Analysis) is required.