:LTESt:MEASure:SIMage:FNAMe:USTandard
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MEASure:SIMage:FNAMe:USTandard
Description
Resets the file name for the screen image file from using a custom name to using the standard name in the following form:
Screen_<date><autonumber>.<extension>
For example, Screen_2017-04-08_1.jpg. Refer to :LTESt:MEASure:SIMage:FNAMe to learn about standard and custom names.
Requires FlexDCA revision A.05.70 and above.