:LTESt:MEASure:SIMage:STATe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MEASure:SIMage:STATe {ON | OFF | 1 | 0}
Query Syntax
:LTESt:MEASure:SIMage:STATe?
Query Response
{1 | 0}
Description
Selects to save a screen image to a file after the specified number of measurement failures stops the limit test. You specify the number of failures required for each individual measurement using the :LTESt:MEASure:<mode>:LOCation:FAILures child command. For example,
:LTESt:MEASure:EYE:LOCation3:FAILures
Information on identifying the measurement is found in the introduction to the limit test programming subsystem. Use the commands shown in the following table to configure the output file.
| Task | Command |
|---|---|
| Enter the filename and path | :LTESt:MEASure:SIMage:FNAMe
|
| Enter the graphics file type | :LTESt:MEASure:SIMage:FTYPe
|
| Select portion of FlexDCA display to capture | :LTESt:MEASure:SIMage:WINDow
|
| Include metadata in jpg and tiff files. | :LTESt:MEASure:SIMage:IMITadata
|
| Invert background color | :LTESt:MEASure:SIMage:INVert
|
| Black and white output | :LTESt:MEASure:SIMage:MONochrome
|
| Capture a single waveform among several displayed waveforms | :LTESt:MEASure:SIMage:SINCLude
|