:LTESt:MEASure:SIMage:SINClude
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MEASure:SIMage:SINClude {ALL | CHANnel{1:8}{A|B|C|D} | FUNCtion{1:64} | WMEMory{1:4} | CGMemroy{1:4}}
Query Syntax
:LTESt:MEASure:SIMage:SINClude?
Description
Selects all or only one of the displayed waveforms to be included on a saved image file when reporting a screen capture for a measurement limit test. By default, all waveforms visible on the display are saved in the screen capture. However, when you select one waveform, all other waveform's will be hidden except for their ground markers (
), which are shown on the screen's right side. Including these markers serves as a reminder that other waveforms were present on the display. Use the :LTESt:MEASure:SIMage:STATe command to enable and disable screen-capture reporting.