:LTESt:MTESt:SIMage:STATe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MTESt:SIMage:STATe {ON | OFF | 1 | 0}
Query Syntax
:LTESt:MTESt:SIMage:STATe?
Query Response
{1 | 0}
Description
Selects to save a screen image to a file after the specified number of mask failures stops the limit test. Use the :LTESt:MTESt:MRESult:FaILures command to specify the number of failures. Use the commands shown in the following table to configure the output file.
| Task | Command |
|---|---|
| Enter the filename and path | :LTESt:MTESt:SIMage:FNAMe
|
| Enter the graphics file type | :LTESt:MTESt:SIMage:FTYPe
|
| Select portion of FlexDCA display to capture | :LTESt:MTESt:SIMage:WINDow
|
| Include metadata in jpg and tiff files. | :LTESt:MTESt:SIMage:IMITadata
|
| Invert background color | :LTESt:MTESt:SIMage:INVert
|
| Black and white output | :LTESt:MTESt:SIMage:MONochrome
|
| Capture a single waveform among several displayed waveforms | :LTESt:MTESt:SIMage:SINCLude
|