:LTESt:MEASure:AMPLitude:LOCation:UPACtion
Removed command for revision A.03.00 and above. This command is no longer available. Use :LTESt:MEASure:MLIMit:UPACtion
insead.
Command Syntax
:LTESt:MEASure:AMPLitude:LOCation{1:32}:UPACtion {FAIL | PASS | IGNore}
Query Syntax
:LTESt:MEASure:AMPLitude:LOCation{1:32}:UPACtion?
Description
Selects an action to be taken if the amplitude measurement limit test in Jitter/Noise mode cannot be performed. The amplitude measurement is identified by a number, from 1 to 32, that is appended to the :LOCation
portion of the command. Refer to the :MEASure:AMPLitude:LOCation:STATe command to learn how to identify the measurement and to turn the measurement limit test on or off.
- FAIL
- If the measurement cannot be made, for example when an edge is expected to be present and is not found, the total number of waveforms is incremented and the total number of failures is incremented. This is the mode to use for most applications.
- PASS
- If the measurement cannot be performed, pass the measurement and do not count it as a failure. The total number of waveforms measured is incremented, but the total number of failures is not.
- IGNore
- If the measurement cannot be performed, ignore the measurement and do not count it as a pass or fail.
IGNore
is similar toPASS
, except the totals for the number of waveforms and failures are not incremented. Therefore, the total indicates the number of tests when the measurement was made.
Use the following sibling commands to configure the measurement:
:FAILures
defines the number of failures for stopping a limit test:FREGion
selects when to fail a measurement:LLIMit
defines the lower limit for failing a measurement:ULIMit
defines the upper limit for failing a measurement
FlexDCA must be in Jitter/Noise mode with amplitude measurements enabled.
Requires Jitter Mode with additional Advanced Amplitude Analysis/RIN/Q-Factor license .