:LTESt:MEASure:AMPLitude:LOCation:FAILures
Removed command for revision A.03.00 and above. This command is no longer available. Use :LTESt:MEASure:MLIMit:FAILures
insead.
Command Syntax
:LTESt:MEASure:AMPLitude:LOCation{1:32}:FAILures <number>
<number> is an int.
Query Syntax
:LTESt:MEASure:AMPLitude:LOCation{1:32}:FAILures?
Description
Sets the number of failures required to stop an amplitude measurement limit test in Jitter/Noise mode. The amplitude measurement is identified by a number, from 1 to 32, that is appended to the :LOCation
portion of the command. Refer to the :MEASure:AMPLitude:LOCation:STATe command to learn how to identify the measurement and to turn the measurement limit test on or off. Use the following sibling commands to configure the measurement:
:FREGion
selects when to fail a measurement:LLIMit
defines the lower limit for failing a measurement:ULIMit
defines the upper limit for failing a measurement:UPACtion
selects an action if the measurement cannot be performed
FlexDCA must be in Jitter/Noise mode with amplitude measurements enabled.
Requires Jitter Mode with additional Advanced Amplitude Analysis/RIN/Q-Factor license .