:LTESt:MEASure:AMPLitude:LOCation:ULIMit
Removed command for revision A.03.00 and above. This command is no longer available. Use :LTESt:MEASure:MLIMit:ULIMit
insead.
Command Syntax
:LTESt:MEASure:AMPLitude:LOCation{1:32}:ULIMit <limit>
<limit> is a double.
Query Syntax
:LTESt:MEASure:AMPLitude:LOCation{1:32}:ULIMit?
Description
Defines the upper limit for the amplitude measurement limit test in Jitter/Noise mode. For example, if you chose to measure total interference and want the largest acceptable value to be 40 mv, set the lower limit to 0 mv and the upper limit to 40 mv, and then set the limit test to fail when the signal is outside the specified limit.
The amplitude measurement is identified by a number, from 1 to 32, that is appended to the :LOCation
portion of the command. Refer to the :MEASure:AMPLitude:LOCation:STATe command to learn how to identify the measurement and to turn the measurement limit test on or off. Use the following sibling commands to configure the measurement:
:FAILures
defines the number of failures for stopping a limit test:FREGion
selects when to fail a measurement:LLIMit
defines the lower limit for failing a measurement:UPACtion
selects an action if the measurement cannot be performed
FlexDCA must be in Jitter/Noise mode with amplitude measurements enabled.
Requires Jitter Mode with additional Advanced Amplitude Analysis/RIN/Q-Factor license .