:MEASure:AMPLitude:EHEight:SOURce
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude
Command Syntax
:MEASure:AMPLitude:EHEight:SOURce <source_waveform>
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}DIFF{1:4}CGMemory{1:8}FUNCtion{1:16}
Query Syntax
:MEASure:AMPLitude:EHEight:SOURce?
Description
Selects the source waveform on which to perform the EHEight measurement.
Requires FlexDCA revision A.05.60 and above.