:MEASure:AMPLitude:EHEight

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude

Command Syntax

:MEASure:AMPLitude:EHEight

Query Syntax

:MEASure:AMPLitude:EHEight?

Description

Returns the NRZ Eye Height measurement on the specified eye. The results are placed in the Amplitude table. This measurement can be made on PAM4 waveforms. See the sidebar in this topic. On PAM4 signals, use the :MEASure:AMPLitude:EHEight:EYE command to select returning the measurement on one of three possible eyes (Eye 0/1, Eye 1/2, or Eye 2/3). The results are placed in the Eye table.

If the table is not already displayed, a "−221, Settings conflict" error message is generated. The query form of the command returns the measured value. Use the :MEASure:AMPLitude:DEFine:ANALysis command to turn on Amplitude analysis and to display the Amplitude table. The query form of the command returns the measured value.

NRZ Waveform

PAM4 Waveform

Measurement Identification

Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.

For example, to return the status of the measurement, :MEASure:AMPLitude:EHEight

flex.write(':MEASure:AMPLitude:EHEight:SOURce CHAN1A')
if flex.query(':MEASure:AMPLitude:EHEight:STATus?') == 'CORR';
    measurement = flex.query(':MEASure:AMPLitude:EHEight?')
else:
	details = flex.query(':MEASure:AMPLitude:EHEight:STATus:DETails?')
	reason = flex.query(':MEASure:AMPLitude:EHEight:STATus:REASon?')

Child commands for measurement identification:

  • :MEASure:AMPLitude:EHEight:SOURce

Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.

Requires FlexDCA revision A.05.60 and above.

Measurement Ready?

To confirm that the measurement is ready to read, you can query the measurement's status:

if ('CORR' in Flex.query(':MEASure:AMPLitude:EHEight:STATus?')):
	measurement = Flex.query(':MEASure:AMPLitude:EHEight?')

If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:MEASure:AMPLitude:EHEight:COUNt?). The technique uses the :COUNt? common measurement query. For example,

if (Flex.query(':MEASure:AMPLitude:EHEight:COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
	measurement = Flex.query(':MEASure:AMPLitude:EHEight?')

You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.

Common Measurement Child Queries

This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.