:MEASure:AMPLitude:EHEight:EYE

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude

Command Syntax

:MEASure:AMPLitude:EHEight:EYE {EYE0 | EYE1 | EYE2}

Query Syntax

:MEASure:AMPLitude:EHEight:EYE?

Description

This command selects the PAM4 eye on which to perform the :EHEight measurement. The query form of the command returns the currently selected eye. This is a command for PAM4 signals only. For NRZ signals, this command results in an "−221, Settings conflict " error.

Requires FlexDCA revision A.05.60 and above.