:MEASure:AMPLitude:ISISymbol:HIGHest?

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude

Query Syntax

:MEASure:AMPLitude:ISISymbol:HIGHest {ONE | ZERO}?

Description

Moves the measurement to the top of the table. Displays the measurement if it is not already shown on the table. The query form of the command returns the measured value.

Returns comma-separated values (string) for the highest measured one or zero in the ISI vs. symbol graph. The string includes the symbol number followed by the ISI value, for example "70,-8.579983e-014". The ISI value has units of volts, Watts, or unit amplitude as specified by the :MEASure:AMPLitude:DEFine:UNITs command.

The ISI vs BIT graph does not need to be displayed before data can be returned from this query.

Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.

Requires FlexDCA revision A.05.60 and above.

This command replaces deprecated command :MEASure:AMPLitude:ISIVsbit:HIGHest?.