:MEASure:AMPLitude:LIST:REMove

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude

Command Syntax

:MEASure:AMPLitude:LIST:REMove <index>

<index> is an int.

Description

Removes the selected interference measurement from the active measurement list, which is displayed in the Amplitude results table. The argument is an index number that specifies the measurement to be removed. The active measurement list is indexed starting at 1. As a result, the first (top most) measurement in the list is identified as 1, the second measurement from the top is identified as 2, and so forth. To get the index value for a specific measurement, use the :LOCation? child command for the targeted measurement. For example, use :MEASure:AMPLitude:Q:LOCation?.

Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.

Example Command Sequence

Read the location of the Q result in the table, send the REMove command with the returned value. In this case 2.

:SYSTem:MODE JITTer
:MEASure:AMPLitude:DEFine:ANALysis ON
:MEASure:AMPLitude:Q:LOCation?
…
…
:MEASure:AMPLitude:LIST:REMove 2