:MEASure:AMPLitude:LIST:DEFault
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude
Command Syntax
:MEASure:AMPLitude:LIST:DEFault
Description
Resets the Amplitude results table to show the default active measurement list in the table.
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.
Example Command Sequence
:SYSTem:MODE JITTer :MEASure:AMPLitude:DEFine:ANALysis ON :MEASure:AMPLitude:LIST:DEFault