:MEASure:AMPLitude:SERFloor?
Command Syntax
:MEASure:AMPLitude:SERFloor
Query Syntax
:MEASure:AMPLitude:SERFloor?
Description
For NRZ measurements, moves the SER floor measurement to the top of the Amplitude table. Displays the measurement if it is not already shown on the table. The query form of the command returns the measured value.
This measurement can be made on PAM4 waveforms. See the sidebar in this topic. On PAM4 signals, use the :MEASure:AMPLitude:SERFloor:EYE command to select returning the measurement on one of three possible eyes (Eye 0/1, Eye 1/2, or Eye 2/3).
The measured SER is the extrapolated SER at the center of the eye. If both amplitude and jitter analysis is active, it will take into account both the probability of timing errors (jitter) as well as the probability of amplitude errors (noise and interference). SER Floor is the predicted SER at intersection of the jitter and amplitude measurement locations within the eye. It accounts for both horizontal eye closure (jitter) and vertical eye closure (noise and interference). The SER floor is calculated by extrapolating the amplitude bathtub curve to the jitter measurement location and extrapolating the jitter bathtub curve to the amplitude measurement location. These floors are then added together to form the SER floor. If the floor is below 10−18, the signal is considered error free.
NRZ Waveform
PAM4 Waveform
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement, :MEASure:AMPLitude:SERFloor?
flex.write(':MEASure:AMPLitude:SERFloor?:SOURce CHAN1A')
if flex.query(':MEASure:AMPLitude:SERFloor?:STATus?') == 'CORR';
measurement = flex.query(':MEASure:AMPLitude:SERFloor??')
else:
details = flex.query(':MEASure:AMPLitude:SERFloor?:STATus:DETails?')
reason = flex.query(':MEASure:AMPLitude:SERFloor?:STATus:REASon?')
Child commands for measurement identification:
:MEASure:AMPLitude:SERFloor?:SOURce
Requires FlexDCA revision A.05.60 and above.
This command replaces deprecated command :AMPLitude:BERFloor.
Example Command Sequence
:MEASure:AMPLitude:DEFine:ANALysis ON :MEASure:AMPLitude:SERFloor:SOURce CHAN1A :MEASure:AMPLitude:SERFloor :MEASure:AMPLitude:SERFloor?
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':MEASure:AMPLitude:SERFloor?:STATus?')):
measurement = Flex.query(':MEASure:AMPLitude:SERFloor??')
If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:MEASure:AMPLitude:SERFloor?:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Flex.query(':MEASure:AMPLitude:SERFloor?:COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
measurement = Flex.query(':MEASure:AMPLitude:SERFloor??')
You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.