:MEASure:CRECovery:TJ:LOCation?
Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4
Query Syntax
:MEASure:CRECovery:TJ:LOCation?
Description
Returns an index for the location of the JSA total jitter TJ (rms) measurement results in the active measurement list. The index is used to select the measurement for limit testing using the :LTESt:MEASure:MLIMit:SOURce:LOCation <index> command.
The returned location index is not used to clear or remove the measurement result as with other measurements in the :MEASure subsystem.
Requires FlexDCA revision A.01.70 and above.