:MEASure:EYE:TJ:RJSValue
Deprecated command. For FlexDCA revision A.05.30 and above, use the :MEASure:EYE:TJ:RJSValue:EYE command instead.
Command Syntax
:MEASure:EYE:TJ:RJSValue <random_jitter>
<random_jitter> is a double.
Query Syntax
:MEASure:EYE:TJ:RJSValue?
Description
Enters the value of RJ used for RJ stabilization. To measure the RJ, switch the N1000A to Jitter Mode and measure the RJ while using a signal that has a short pattern. Or, measure the RJ using a separate instrument, such as a spectrum analyzer. Use the :MEASure:EYE:TJ:RJSTabilize command to turn on or off the use of RJ stabilization.
The following table shows that the eye mode DJ, Jn, RJ, and TJ measurements each have RJSTabilize and RJSValue child commands. Because the RJSTabilize commands control the same setting, you can use any of the four commands to turn RJ stabilization on or off. Also, because the RJSValue commands enter or query the same variable, you can use any of the four commands to change or query the RJ value.
Equivalent RJ Stabilization (On / Off) Commands
- :MEASure:EYE:DJ:RJSTabilize
- :MEASure:EYE:JN:RJSTabilize
- :MEASure:EYE:RJ:RJSTabilize
- :MEASure:EYE:TJ:RJSTabilize
Equivalent RJ Value Commands
Requires Option 401, Advanced Eye Analysis Software license.
Requires FlexDCA revision A.02.50 and above.