:MEASure:EYE:TJ:RJSTabilize

Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
Licensed Feature:
F-AEYE
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:TJ:RJSTabilize {ON | OFF}

Query Syntax

:MEASure:EYE:TJ:RJSTabilize?

Description

Turns on or off RJ stabilization. When RJ stabilization is on, use the :MEASure:EYE:TJ:RJSValue command to enter the RJ value. To measure the RJ, switch the N1000A to Jitter Mode and measure the RJ while using a signal that has a short pattern. Or, measure the RJ using a separate instrument, such as a spectrum analyzer. The following lists show that the eye mode DJ, Jn, RJ, and TJ measurements each have RJSTabilize and RJSValue child commands. Because the RJSTabilize commands control the same setting, you can use any of the four commands to turn RJ stabilization on or off. Also, because the RJSValue commands enter or query the same variable, you can use any of the four commands to change or query the RJ value.

Equivalent RJ Stabilization (On / Off) Commands

Equivalent RJ Value Commands

Requires Option 401, Advanced Eye Analysis Software license.

Requires FlexDCA revision A.02.50 and above.