:MEASure:EYE:EHEight
Command Syntax
:MEASure:EYE:EHEight
Query Syntax
:MEASure:EYE:EHEight?
Description
Moves the Eye height measurement to the top of the Results table. Displays the measurement if it is not already shown on the table. The query form of the command returns the measured value. Eye height is a measure of the vertical opening of an eye diagram. An ideal eye opening would be measured from the one level to the zero level. However, noise on the eye will cause the eye to close. The eye height measurement determines eye closure due to noise. Sources can be any displayed waveform, color-grade memory, or function. For example, CHAN1A, CGMemory1, or FUNCtion1. Use the :MEASure:EBOundary:LEFT, :MEASure:EBOundary:RIGHt, and :MEASure:EBOundary:DEFault commands to change the eye boundary settings.
This Eye mode measurement can be applied to NRZ waveforms but not PAM4 waveforms.
Child commands for measurement identification:
:MEASure:EYE:EHEight:SOURce:MEASure:EYE:EHEight:FORMat
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement, :MEASure:EYE:EHEight
flex.write(':MEASure:EYE:EHEight:SOURce CHAN1A')
if flex.query(':MEASure:EYE:EHEight:STATus?') == 'CORR';
measurement = flex.query(':MEASure:EYE:EHEight?')
else:
details = flex.query(':MEASure:EYE:EHEight:STATus:DETails?')
reason = flex.query(':MEASure:EYE:EHEight:STATus:REASon?')
Example Command Sequence
:MEASure:EYE:EHEight:SOURce CHAN1A :MEASure:EYE:EHEight :MEASure:EYE:EHEight?
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':MEASure:EYE:EHEight:STATus?')):
measurement = Flex.query(':MEASure:EYE:EHEight?')
If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:MEASure:EYE:EHEight:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Flex.query(':MEASure:EYE:EHEight:COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
measurement = Flex.query(':MEASure:EYE:EHEight?')
You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.