:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RJSValue:EYE

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4/6/8

Command Syntax

:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RJSValue:EYE{0|1|2} <random_jitter>

<random_jitter> is a double.

Query Syntax

:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RJSValue:EYE{0|1|2}?

Description

For Random Jitter (RJ) stabilization, sets the value of RJ for the selected eye on Eye Width and Eye Height measurements. To measure the RJ, switch the N1000A to Jitter Mode and measure the RJ while using a signal that has a short pattern. Or, measure the RJ using a separate instrument. Use the :MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RJSTabilize command to turn on or off the use of RJ stabilization.

Command Description
:EYE2 Applies to eye 2/3.
:EYE1
(or :EYE)
Applies to eye 1/2.
:EYE0 Applies to eye 0/1.

Linked RJ Stabilization (On / Off) Commands

The Eye Width and Eye Height RJSTablilize are equivalent.

Linked RJ Value Commands

The RJSValue:EYE commands for the same eye level for Eye Width and Eye Height measurements are equivalent. Use one of a commands to enter a value for one level on a measurement and it is changed on both measurements. For example, enter the eye two value for an Eye Height measurement and the eye two value is also entered for for an Eye Width measurement.

Requires FlexDCA revision A.05.30 and above.