:MEASure:EYE:PAM:PMIN:STATus:DETails?
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8
Query Syntax
:MEASure:EYE:PAM:PMIN:STATus:DETails?
Description
Returns a string that may provide additional details for a failed :EYE:PAM:PMIN measurement. If the measurement was successful, a null string is returned.
For a basic description of a measurement failure, use the :EYE:PAM:PMIN:STATus:REASon?. Use the :EYE:PAM:PMIN:STATus? parent query to determine if the measurement has failed.
Requires FlexDCA revision A.07.60 and above.