:MEASure:EYE:PAM:PMIN:UNITs
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:EYE:PAM:PMIN:UNITs {WATT | DBM}
Query Syntax
:MEASure:EYE:PAM:PMIN:UNITs?
Description
Sets the amplitude units for the Pk-Pk Amplitude measurement (:MEASure:EYE:PAM:PMIN). Units can be Watts (WATT) or dBM (DBM).
Requires FlexDCA revision A.07.60 and above.